Hello,
I would like to use the HRPWM on an F28334 running at 150MHz.
I use SFO_TI_Build_V5B_fpu.lib
At power up, I make initialization and get a MepScale of 49. During operation I regularly update the MepScale with the calibration function and get about 46.
However, if using 46 for the MepScale, I get jumps at my output signal at the low resolution PWM transitions.
I could remove those jumps by setting the MepScale to 52. Therefore, it seems to me that the calibration function should return this value and not 46. I am not sure it would be a good thing to hard code a value as the datasheet says it is temperature and voltage dependent.
Is there something that I can do to improve the calibration ?
Thanks