Hello
When I call to CCS3.1 and connect to my target, the PC jump to the reset address 3FFC00.
In this situation I can set up to 2 breakpoints everywhere: in ROM, in Flash, etc...
In order to "synchronize" the target to its code I load the 'RAM only' with On-Chip Flash Programmer.
From now, the system doesn't allow me to set any breakpoint, and I need to set at least one breakpoint to debug.
Is there something to do about this?
Thank you.