Hello i like to generate c-Code with the Embedded Coder,
if I type "checkEnvSetup('ccsv5',f28027','check') it says:
2802x C/c++ Header Files: Your Version: 2.10 Required Version 1.29 Required for Code generation....
if I Build My model, the Error : "could not not open source file "DSP2802x_Examples.h" , this happens because in the header Files i use the header file is named "F2802x_examples.h"....
If i add the required version 1.29 i cathc the error "Variable PartIdRegs was declared with a never completed type " that problem was answered in another thread that the usage of this old version is incorrect.
so I thing that i have to tell matlab to change the Required version of the Header files.... am I right, and how is this done??
Thanks for your Help