hi:
I use motorware 2b project run from flash ,but it is fail,
I opened 2b lab project FLASH. and changed the CMD.file as F28069M ,and add the "memcopy.c" , then build complishment.
then load to my board, debug runing is ok.
but ,I disconnect the simulator. regain power up . I find 28069M doesn't run form flash .
I have let GPIO34. GPIO37 connect high signal when MCU rest time.
I don't know why it doesn't run from flash . maybe somewhere I operated wrong. help me!