Hi,
I have a problem when sending serial from hercules emulator to F28335 using SCI communication.
I use code from C2000 teaching rom from TI which is Lab9_4.c. The code should wait for character 'Texas' to be received and reply with 'Insturments!' to terminal. The program works find, i.e responds, when I send character one by one by typing 'T' in hercules then send, type 'e' then send and so on. But if I type 'Texas' in hercules and then click send, the program don't send the response.
I check the content of variable buffer when the program generate receive interrupt. when I type character 'Texas' on hercules and click send the contents are:
buffer[0] = 'T', buffer[1] = '.', buffer[2] = '.', buffer[3] = 'X', buffer[4] = '.'
I use:
Board: Technosoft MSK28335
CCS version 4.1.2
terminal emulator: Hercules
the code I use:
// // Lab9_4: TMS320F28335 // (c) Frank Bormann // //########################################################################### // // FILE: Lab9_4.c // // TITLE: DSP28 SCI - Communication to PC - Terminal // SCI-Setup: 9600 Baud, 8 Bit , ODD Parity , 1 Stopbit // SCI - TX and RX - Interrupt are used in this Lab // SCI - TX and RX - FIFO are used in this Lab // DSP waits for "Texas" and answers with "Instruments" // Watchdog active , serviced solely in main-loop //########################################################################### // Ver | dd mmm yyyy | Who | Description of changes // =====|=============|======|=============================================== // 3.0 | 08 Jul 2009 | F.B. | adapted for ControlCard28335 @ 20MHz // 3.1 | 15 Nov 2009 | F.B | Lab9_4 for F28335 @30MHz and PE revision 5 //########################################################################### #include "DSP2833x_Device.h" #include <string.h> // External Function prototypes extern void InitSysCtrl(void); extern void InitPieCtrl(void); extern void InitPieVectTable(void); // Prototype statements for functions found within this file. void Gpio_select(void); void SCIA_init(void); interrupt void SCIA_TX_isr(void); // SCI-A Transmit Interrupt Service interrupt void SCIA_RX_isr(void); // SCI-A Receive Interrupt Service // Global Variables char message[]={" Instruments! \n\r"}; //########################################################################### // main code //########################################################################### void main(void) { InitSysCtrl(); // Basic Core Initialization // SYSCLK=150MHz, HISPCLK=75MHz, LSPCLK=37.5MHz EALLOW; SysCtrlRegs.WDCR= 0x00AF; // Re-enable the watchdog EDIS; // 0x00E8 to disable the Watchdog , Prescaler = 1 // 0x00AF to NOT disable the Watchdog, Prescaler = 64 Gpio_select(); // GPIO9, GPIO11, GPIO34 and GPIO49 as output // to 4 LEDs at Peripheral Explorer InitPieCtrl(); // default status of PIE; in DSP2833x_PieCtrl.c InitPieVectTable(); // init PIE vector table; in DSP2833x_PieVect.c // re-map PIE - entry for SCI-A-TX and SCI-A-RX EALLOW; PieVectTable.SCITXINTA = &SCIA_TX_isr; PieVectTable.SCIRXINTA = &SCIA_RX_isr; EDIS; SCIA_init(); // Initalize SCI // Enable SCI-A TX Interrupt Group9 interupt 2 PieCtrlRegs.PIEIER9.bit.INTx2 = 1; // Enable SCI-A RX Interrupt Group9 interupt 1 PieCtrlRegs.PIEIER9.bit.INTx1 = 1; // Enable INT9 for SCIA-TX and SCIA-RX: IER = 0x100; // Enable global Interrupts and higher priority real-time debug events: EINT; // Enable Global interrupt INTM ERTM; // Enable Global realtime interrupt DBGM while(1) { EALLOW; SysCtrlRegs.WDKEY = 0x55; // Service watchdog #1 SysCtrlRegs.WDKEY = 0xAA; // Service watchdog #2 EDIS; } } void Gpio_select(void) { EALLOW; GpioCtrlRegs.GPAMUX1.all = 0; // GPIO15 ... GPIO0 = General Puropse I/O GpioCtrlRegs.GPAMUX2.all = 0; // GPIO31 ... GPIO16 = General Purpose I/O GpioCtrlRegs.GPAMUX2.bit.GPIO28 = 1; // SCIRXDA GpioCtrlRegs.GPAMUX2.bit.GPIO29 = 1; // SCITXDA GpioCtrlRegs.GPBMUX1.all = 0; // GPIO47 ... GPIO32 = General Purpose I/O GpioCtrlRegs.GPBMUX2.all = 0; // GPIO63 ... GPIO48 = General Purpose I/O GpioCtrlRegs.GPCMUX1.all = 0; // GPIO79 ... GPIO64 = General Purpose I/O GpioCtrlRegs.GPCMUX2.all = 0; // GPIO87 ... GPIO80 = General Purpose I/O GpioCtrlRegs.GPADIR.all = 0; GpioCtrlRegs.GPADIR.bit.GPIO9 = 1; // peripheral explorer: LED LD1 at GPIO9 GpioCtrlRegs.GPADIR.bit.GPIO11 = 1; // peripheral explorer: LED LD2 at GPIO11 GpioCtrlRegs.GPBDIR.all = 0; // GPIO63-32 as inputs GpioCtrlRegs.GPBDIR.bit.GPIO34 = 1; // peripheral explorer: LED LD3 at GPIO34 GpioCtrlRegs.GPBDIR.bit.GPIO49 = 1; // peripheral explorer: LED LD4 at GPIO49 GpioCtrlRegs.GPCDIR.all = 0; // GPIO87-64 as inputs EDIS; } void SCIA_init() { SciaRegs.SCICCR.all =0x0027; // 1 stop bit, No loopback // ODD parity,8 char bits, // async mode, idle-line protocol SciaRegs.SCICTL1.all =0x0003; // enable TX, RX, internal SCICLK, // Disable RX ERR, SLEEP, TXWAKE // SYSCLOCKOUT = 150MHz; LSPCLK = 1/4 = 37.5 MHz // BRR = (LSPCLK / (9600 x 8)) -1 // BRR = 487 gives 9605 Baud SciaRegs.SCIHBAUD = 487 >> 8; // Highbyte SciaRegs.SCILBAUD = 487 & 0x00FF; // Lowbyte SciaRegs.SCICTL2.bit.TXINTENA = 1; // enable SCI-A Tx-ISR SciaRegs.SCICTL2.bit.RXBKINTENA = 1; // enable SCI_A Rx-ISR SciaRegs.SCIFFTX.all = 0xC060; // bit 15 = 1 : relinquish from Reset // bit 14 = 1 : Enable FIFO // bit 6 = 1 : CLR TXFFINT-Flag // bit 5 = 1 : enable TX FIFO match // bit 4-0 : TX-ISR, if TX FIFO is 0(empty) SciaRegs.SCIFFCT.all = 0x0000; // Set FIFO transfer delay to 0 SciaRegs.SCIFFRX.all = 0xE065; // Rx interrupt level = 5 SciaRegs.SCICTL1.all = 0x0023; // Relinquish SCI from Reset } // SCI-A Transmit Interrupt Service interrupt void SCIA_TX_isr(void) { unsigned int i; // copy 16 character into SCI-A TX buffer for(i=0;i<16;i++) SciaRegs.SCITXBUF= message[i]; // Acknowledge this interrupt to receive more interrupts from group 9 PieCtrlRegs.PIEACK.all = PIEACK_GROUP9; } // SCI-A Receive Interrupt Service interrupt void SCIA_RX_isr(void) { int i; char buffer[16]; for (i=0;i<16;i++) buffer[i]= SciaRegs.SCIRXBUF.bit.RXDT; if (strncmp(buffer, "Texas", 5) == 0) { SciaRegs.SCIFFTX.bit.TXFIFOXRESET =1; // enable TXFIFO SciaRegs.SCIFFTX.bit.TXFFINTCLR = 1 ; // force TX-ISR } SciaRegs.SCIFFRX.bit.RXFIFORESET = 0; // reset RX-FIFO pointer SciaRegs.SCIFFRX.bit.RXFIFORESET = 1; // enable RX-operation SciaRegs.SCIFFRX.bit.RXFFINTCLR = 1; // clear RX-FIFO INT Flag PieCtrlRegs.PIEACK.all = PIEACK_GROUP9; } //=========================================================================== // End of SourceCode. //===========================================================================
It would be helpful if someone could give any suggestion or information to this problem
Thanks