Hi,
I'm using SDFlash version 1.2 that is set up for a TMS320F241 DSP and XDS510PP Plus emulator. When I do only a Verify (Erase and Program are not selected), I get the following error:
ERR: Verify target algorithm failed.
ERR: Failed at block address 0x00000810.
ERR: Verify flash failed.
I looked at the flash target memory dump and found a data discrepancy with a 16-bit word at address 0x000008AC. I am wondering where did 0x00000810 come from? It sounds like it's the start of a block but the verify algorithm code specifies that the program buffer size (PRG_bufsize) is set to 200 which doesn't make sense with it failing at 0x00000810. I was assuming each block should be of size 200 words, so the block address that it fails on should be aligned with this.
I know I'm overlooking something trivial. Can someone clarify this?