I have written a simple program for the F28027 lauchpad, which has 2 functions: (1) send increasing number through uart every second; (2) use an interrupt to receive a num from the computer through uart and send back. The program is written into flash and run in RAM.
the problem is: the launchpad is powered by the usb, so when the usb is connected, the dsp is started, and the program is running ,but the interrupt is not functional(function 2 is not work). And after I push the reset button, the function is running good. so is this a program problem or is the pad's characteristic: we must push the reset button to let the program work normally? if this is a program problem, what's the difference between the usb powerup and the rst?
thank you~