From my customer -
I have a question about implementing an IIR filter in the TMS32F028069.
I am using the FixedPoint Library v1.01 and attempting to use the iir16 filter.
I computed the filter coefficients using the matlab script, and generally followed the implementation example in the controlSUITE folder.
As I learned from this discussion here: http://e2e.ti.com/support/microcontrollers/c2000/f/171/t/204289.aspx
There is a divide by 2 in the output of the filter, which otherwise appears undocumented. That aside, I was able to get answers that I would expect when running the code on the target with the debugger, but when I went to run without the debugger I was getting completely unreasonable values. I have allocated memory in .cmd file as outlined in the example for both the filter itself and the data buffer. Any ideas or threads to follow as to why I am getting a different response?
I can send code snippets etc. as needed.