This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS329F28027 feedforward operation

Using TMS320F28027  Piccolo in off-line 3-ph BLDC motor drive, approx. 25 Watts, Fsw = 20kHz.  We want to use a passive valley fill rectifier front end at 50% ripple voltage.  Is there a way to adjust the feed forward DC bus input to the Piccolo to reject the 120Hz DC bus ripple?  Using the EVM we start getting appreciable 120hz feed through of the rectified mains when we have greater than 15% input voltage ripple.