Hello:
I'm trying to generate a Motorola s3 format file (32bits address) for the ARM M3 .out file. The following post build command is performed:
armhex -m3 -o MyM3Prog.s37 MyM3Prog.out
I get the following files:
1. MyM3Prog.s37
2. MyM3Prog.m1
3. MyM3Prog.m2
4. MyM3Prog.m3
It seems that the MyM3Prog.s37 is OK but what are the other file? Any use for them or what is the purpose for them?
Regards Arye