We are using a DRV8301 motor control kit with a Piccolo 28069 control card, ccs 5.4, and compiler 6.2.7.
Because of an accident the control card lost the usb connector along with some copper traces. We had a spare BlackHawk xds100v2-ARM emulator, with 20 and 10 ARM pinout, so we are trying to use it to continue the development.
We assembled a cable using the following schematic from tincan tools as a guide.
When trying to program the device using TI XDS100v2 USB EMULATOR / TMS320F28069 target configuration we run into the following error:
Error connecting to the target: (Error -1015 @ 0x0) Device is not responding to the request. Device may be locked, or the emulator connection may be unreliable. Unlock the device if possible, and power-cycle the board. If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.1.73.0)
Running a JTAG connection test we have the following output:
[Start] Execute the command: %ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity [Result] -----[Print the board config pathname(s)]------------------------------------ C:\Users\Juanjo\AppData\Local\.TI\693494126\ 0\0\BrdDat\testBoard.dat -----[Print the reset-command software log-file]----------------------------- This utility has selected a 100- or 510-class product. This utility will load the adapter 'jioserdesusb.dll'. The library build date was 'Apr 1 2013'. The library build time was '23:55:08'. The library package version is '5.1.73.0'. The library component version is '35.34.40.0'. The controller does not use a programmable FPGA. The controller has a version number of '4' (0x00000004). The controller has an insertion length of '0' (0x00000000). This utility will attempt to reset the controller. This utility has successfully reset the controller. -----[Print the reset-command hardware log-file]----------------------------- The scan-path will be reset by toggling the JTAG TRST signal. The controller is the FTDI FT2232 with USB interface. The link from controller to target is direct (without cable). The software is configured for FTDI FT2232 features. The controller cannot monitor the value on the EMU[0] pin. The controller cannot monitor the value on the EMU[1] pin. The controller cannot control the timing on output pins. The controller cannot control the timing on input pins. The scan-path link-delay has been set to exactly '0' (0x0000). -----[The log-file for the JTAG TCLK output generated from the PLL]---------- There is no hardware for programming the JTAG TCLK frequency. -----[Measure the source and frequency of the final JTAG TCLKR input]-------- There is no hardware for measuring the JTAG TCLK frequency. -----[Perform the standard path-length test on the JTAG IR and DR]----------- This path-length test uses blocks of 512 32-bit words. The test for the JTAG IR instruction path-length failed. The JTAG IR instruction scan-path is stuck-at-zero. The test for the JTAG DR bypass path-length failed. The JTAG DR bypass scan-path is stuck-at-zero. -----[Perform the Integrity scan-test on the JTAG IR]------------------------ This test will use blocks of 512 32-bit words. This test will be applied just once. Do a test using 0xFFFFFFFF. Test 1 Word 0: scanned out 0xFFFFFFFF and scanned in 0x00000000. Test 1 Word 1: scanned out 0xFFFFFFFF and scanned in 0x00000000. Test 1 Word 2: scanned out 0xFFFFFFFF and scanned in 0x00000000. Test 1 Word 3: scanned out 0xFFFFFFFF and scanned in 0x00000000. Test 1 Word 4: scanned out 0xFFFFFFFF and scanned in 0x00000000. Test 1 Word 5: scanned out 0xFFFFFFFF and scanned in 0x00000000. Test 1 Word 6: scanned out 0xFFFFFFFF and scanned in 0x00000000. Test 1 Word 7: scanned out 0xFFFFFFFF and scanned in 0x00000000. The details of the first 8 errors have been provided. The utility will now report only the count of failed tests. Scan tests: 1, skipped: 0, failed: 1 Do a test using 0x00000000. Scan tests: 2, skipped: 0, failed: 1 Do a test using 0xFE03E0E2. Scan tests: 3, skipped: 0, failed: 2 Do a test using 0x01FC1F1D. Scan tests: 4, skipped: 0, failed: 3 Do a test using 0x5533CCAA. Scan tests: 5, skipped: 0, failed: 4 Do a test using 0xAACC3355. Scan tests: 6, skipped: 0, failed: 5 Some of the values were corrupted - 83.3 percent. The JTAG IR Integrity scan-test has failed. -----[Perform the Integrity scan-test on the JTAG DR]------------------------ This test will use blocks of 512 32-bit words. This test will be applied just once. Do a test using 0xFFFFFFFF. Test 1 Word 0: scanned out 0xFFFFFFFF and scanned in 0x00000000. Test 1 Word 1: scanned out 0xFFFFFFFF and scanned in 0x00000000. Test 1 Word 2: scanned out 0xFFFFFFFF and scanned in 0x00000000. Test 1 Word 3: scanned out 0xFFFFFFFF and scanned in 0x00000000. Test 1 Word 4: scanned out 0xFFFFFFFF and scanned in 0x00000000. Test 1 Word 5: scanned out 0xFFFFFFFF and scanned in 0x00000000. Test 1 Word 6: scanned out 0xFFFFFFFF and scanned in 0x00000000. Test 1 Word 7: scanned out 0xFFFFFFFF and scanned in 0x00000000. The details of the first 8 errors have been provided. The utility will now report only the count of failed tests. Scan tests: 1, skipped: 0, failed: 1 Do a test using 0x00000000. Scan tests: 2, skipped: 0, failed: 1 Do a test using 0xFE03E0E2. Scan tests: 3, skipped: 0, failed: 2 Do a test using 0x01FC1F1D. Scan tests: 4, skipped: 0, failed: 3 Do a test using 0x5533CCAA. Scan tests: 5, skipped: 0, failed: 4 Do a test using 0xAACC3355. Scan tests: 6, skipped: 0, failed: 5 Some of the values were corrupted - 83.3 percent. The JTAG DR Integrity scan-test has failed. [End]
Now, setting the target config as XDS100v1 /TMS320f28069, we have the following jtag connection test:
[Start] Execute the command: %ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity [Result] -----[Print the board config pathname(s)]------------------------------------ C:\Users\Juanjo\AppData\Local\.TI\693494126\ 0\0\BrdDat\testBoard.dat -----[Print the reset-command software log-file]----------------------------- This utility has selected a 100- or 510-class product. This utility will load the adapter 'jioserdesusb.dll'. The library build date was 'Apr 1 2013'. The library build time was '23:55:08'. The library package version is '5.1.73.0'. The library component version is '35.34.40.0'. The controller does not use a programmable FPGA. The controller has a version number of '4' (0x00000004). The controller has an insertion length of '0' (0x00000000). This utility will attempt to reset the controller. This utility has successfully reset the controller. -----[Print the reset-command hardware log-file]----------------------------- The scan-path will be reset by toggling the JTAG TRST signal. The controller is the FTDI FT2232 with USB interface. The link from controller to target is direct (without cable). The software is configured for FTDI FT2232 features. The controller cannot monitor the value on the EMU[0] pin. The controller cannot monitor the value on the EMU[1] pin. The controller cannot control the timing on output pins. The controller cannot control the timing on input pins. The scan-path link-delay has been set to exactly '0' (0x0000). -----[The log-file for the JTAG TCLK output generated from the PLL]---------- There is no hardware for programming the JTAG TCLK frequency. -----[Measure the source and frequency of the final JTAG TCLKR input]-------- There is no hardware for measuring the JTAG TCLK frequency. -----[Perform the standard path-length test on the JTAG IR and DR]----------- This path-length test uses blocks of 512 32-bit words. The test for the JTAG IR instruction path-length succeeded. The JTAG IR instruction path-length is 0 bits. The test for the JTAG DR bypass path-length succeeded. The JTAG DR bypass path-length is 0 bits. -----[Perform the Integrity scan-test on the JTAG IR]------------------------ This test will use blocks of 512 32-bit words. This test will be applied just once. Do a test using 0xFFFFFFFF. Scan tests: 1, skipped: 0, failed: 0 Do a test using 0x00000000. Scan tests: 2, skipped: 0, failed: 0 Do a test using 0xFE03E0E2. Scan tests: 3, skipped: 0, failed: 0 Do a test using 0x01FC1F1D. Scan tests: 4, skipped: 0, failed: 0 Do a test using 0x5533CCAA. Scan tests: 5, skipped: 0, failed: 0 Do a test using 0xAACC3355. Scan tests: 6, skipped: 0, failed: 0 All of the values were scanned correctly. The JTAG IR Integrity scan-test has succeeded. -----[Perform the Integrity scan-test on the JTAG DR]------------------------ This test will use blocks of 512 32-bit words. This test will be applied just once. Do a test using 0xFFFFFFFF. Scan tests: 1, skipped: 0, failed: 0 Do a test using 0x00000000. Scan tests: 2, skipped: 0, failed: 0 Do a test using 0xFE03E0E2. Scan tests: 3, skipped: 0, failed: 0 Do a test using 0x01FC1F1D. Scan tests: 4, skipped: 0, failed: 0 Do a test using 0x5533CCAA. Scan tests: 5, skipped: 0, failed: 0 Do a test using 0xAACC3355. Scan tests: 6, skipped: 0, failed: 0 All of the values were scanned correctly. The JTAG DR Integrity scan-test has succeeded. [End]
And when we try to program the device we get the following error:
Error connecting to the target: (Error -1135 @ 0x0) The emulator reported an error. Confirm emulator configuration and connections, reset the emulator, and retry the operation. (Emulation package 5.1.73.0)
So, if we select the right emulator, the jtag test fails, if we select de v1 the jtag test succeds, but either way we CAN'T program the device.
All help is appreciated.
Thanks in advance.