Dear TI Team,
is there any issue why the 'MIIPHY-- GPIO settings' for the M3-Primary-Mode3 and further (see Table 3-28)
are only partly included in the file 'controlSUITE\device_support\f28m36x\v202\MWare\driverlib\gpio.h'?
For instance;
I missing the setting for 'PF6_GPIO46 - MIIRXD2' in file 'gpio.h'
I would expect the setting: #define GPIO_PF6_MIIRXD2 0x00051803
However the setting '#define GPIO_PF6_U1RTS 0x0005180a' is available, which is not mentioned in the Table 3-28.
Will this be updated in a further library version or are the missing pin's are not usable for Ethernet interface?
Thanks
WJ