Hi good day,
I finished my program in this control card and my project operated very well, but i have some inconvenient with the form that is loaded the program in the MCU.
In fact i had my program configurated to operate in real time, i have active the DEBUG option in the build configurations for this, and i can work with my PC. But in this moment i need load the program that i developed in the control card or more exactly in the MCU, for develop this code my project without PC. For this, i changed the build confuguration to active REALISE, and i can work without my PC perfect, but when i turn off the power source of the control card and after this i turn on the power source, the program is lost, the program not are in the MCU. The program is erased when i turn off the power source.
I need that this program can be loaded always in the MCU, independient if i turn off or not the power source of my card. I need that this program can will be save in the MCU alway,
Thanks for your help.
Please tell me if have a solution.
Regards
David Becerra