Dear TI team,
I can not initialze and use the ePWM7-A Module.
In debugging mode (CCS-6), all the ePWM7 registers are still '0' ZERO after the initialisation procedure.
The other PWM Modules 1..6 works as designed for.
Is there any restriction regarding the 'ePWM7'?
Below the initialization procedure.
void c28Pwm7Init( void )
{
EALLOW;
GpioCtrlRegs.GPAMUX1.bit.GPIO12 = 1;
GpioG1CtrlRegs.GPADIR.bit.GPIO12 = 1;
EDIS;
EPwm7Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; /* count up and down */
EPwm7Regs.TBPRD = (Uint16)EPWM7_TIMER_TBPRD; /* set timer period */
EPwm7Regs.CMPA.half.CMPA = (Uint16)EPWM7_MIN_CMPA; /* initial compare A value */
EPwm7Regs.TBCTL.bit.PHSEN = TB_DISABLE; /* disable phase loading */
EPwm7Regs.TBPHS.half.TBPHS = 0x0000; /* phase is 0 */
EPwm7Regs.TBCTR = 0x0000; /* clr counter */
EPwm7Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; /* clock ratio to SYSCLKOUT */
EPwm7Regs.TBCTL.bit.CLKDIV = TB_DIV1;
/* setup shadow register load on ZERO */
EPwm7Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
EPwm7Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
EPwm7Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;
EPwm7Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;
/* disable trip zone */
EALLOW;
EPwm7Regs.TZCTL.bit.TZA = TZ_NO_CHANGE; /* EPwm7A */
EPwm7Regs.TZCTL.bit.TZB = TZ_NO_CHANGE; /* EPwm7B */
EPwm7Regs.TZCTL.bit.DCAEVT1 = TZ_NO_CHANGE;
EPwm7Regs.TZCTL.bit.DCAEVT2 = TZ_NO_CHANGE;
EPwm7Regs.TZCTL.bit.DCBEVT1 = TZ_NO_CHANGE;
EPwm7Regs.TZCTL.bit.DCBEVT2 = TZ_NO_CHANGE;
EDIS;
/* set actions qualifier */
EPwm7Regs.AQCTLA.bit.CAU = AQ_SET;
EPwm7Regs.AQCTLA.bit.CAD = AQ_CLEAR;
} /* end c28Pwm7Init() */
Just note:
The same code was used with the EVM board and the mounted F28M36 experimental chip. There was no issue.
Regards
WJ