please help me.
thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Veera,
Veerabhadra P V said:please help me.
thank you
You can go through the code present here in controlSuite:
C:\ti\controlSUITE\device_support\f2806x\v136\F2806x_examples_ccsv5\flash_f28069
This is a flash based example. Also, here are the steps to convert RAM based code to Flash based:
You need to add these two statements
MemCopy(&RamfuncsLoadStart, &RamfuncsLoadEnd, &RamfuncsRunStart);
InitFlash(); after InitPieVectTable();
Add DSP2806x_MemCopy.c file to the project.
Define extern variables above main() function.
extern Uint16 RamfuncsLoadStart;
extern Uint16 RamfuncsLoadEnd;
extern Uint16 RamfuncsRunStart;
Replace 28069_RAM_lnk.cmd with F28069.cmd
Compile the code.
Configure your GPIO's to boot to flash.
Observe the cmd file and the Example_28069Flash.c file of the above flash sample project.
Regards,
Gautam
Thanks for your reply bro.
I'm still facing problem. It cries out of memory now though flash is 100 times ram.
some bss has to be changed in command file itseems ... please help me.
thank you
Did you replace the .cmd file in your project ie did you use flash based cmd file?