All,
I have this question concerning C2Prog, the flash programming utility from Codeskin. When this tool is used on a LF2407A device, does it read the programmed flash memory and compare the flash image with the one on the PC hard drive? I am concerned about data being corrupted while it is transmitted from the PC’s serial port to SCI port of LF2407A or the RAM buffer (on the 2407A) contents being corrupted.
Hareesh