Hello
Looking into using the HVPSFB_v1.1 Project/Code as the platform for developing a higher power custom design.
Since one of the modes of operation is Peak Current Mode Control (which is what I plan to use) - it should be capable of configuring a parallel mode operation . Any suggestions on best way to implement this ?
I was considering having a current share bus between the two Piccolo's using the SPI interface ?
Thanks
Matt