Can anyone provide me ePWM source code example in c, to generate fixed frequency adjustable between 400Khz-500Khz without any dependency on interrupt or code, ie it has to run alone once configured.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can anyone provide me ePWM source code example in c, to generate fixed frequency adjustable between 400Khz-500Khz without any dependency on interrupt or code, ie it has to run alone once configured.
Hi Richard,
All you've to do is download the zip file from this location and import the ePWM project meant for F2808 controller.
Change the TBPRD value according to the required frequency.
http://www.ti.com/tool/sprc191
Regards,
Gautam