hi team,
A customer, in cc of this post, wants to get the HVMTRPFC kit to work with f28069 control card in place of the documented F28035.
we're stuck at the connection stage as the PC doesnt seem to recognize the xds100 connection on JP1, while all recommendation from userguide where followed.
Customer as ccs installed and did get xds100 connection with other ti kits on the same PC.
I would suspect a jumper setting specific to f28069 controlcard, maybe?
also the 2 crosshair guis (HVMTRPFCKIT-BLDC-GUI and HVMTRPFCKIT-PM-ACI-GUI) generate the same error:
"VCP auto-connection is enabled for this interface, but there was a problem retrieving COM ports from your system. This may be due to a WMI corruption" which makes sense if the XDS100 doesnt appear in windows control panel.
thanks for support