My program runs in 28335 external RAM IS61LV51216, F28335 XD[0..15] connects to RAM's I/O0 ~ I/O15. Now I want to connects a ADC to F28335, using parallel mode, i.e, AD converter data port D[0..15] connects to F28335 XD[16..31], for purpose of using F28335's DMA to mass data aquisition from ADC, ADC is mapped to address of XINTF
is it possible to do so? I want to know that during executing of program, does data exchange between CPU and external RAM(low 16-bits of XD[0..31]) affects data on XD[16..31]? ADC data path from XINTF to DMA works well or not?
Many thanks.