Hello everyone,
I have one question about the ADC and Comparator combined pin. As shown in the datasheet, the CMPIN1P is shared Pin with ADCINA2, and the CMPIN1N is shared Pin with ADCINA3. When i use the internal DAC as the negative input of comparator, that is, it just uses the positive input pin, such as CMPIN1P, So, can the CMPIN1N pin work as the ADCINA3 simultaneously for a single 12-bit ADC input?