I have an f28027 Launchpad and cannot receive any serial data from it, using the demo app. I have:
- checked the COM port
- checked the switches on the launchpad (SCI is on)
- checked that the launchpad is functioning - LEDs are blinking appropriately
- checked the baud rate - 115200 as specified
- checked that both power LEDs are lit
I have tried with two different computers and two different launchpad boards.
I am using RealTerm, which works with other boards.
I see that it seems to be receiving some signals from the board just nothing on Rx.
Anything else I should check?