Hello,
I am running into problems, when trying to adapt PWM frequency with HRPWM within my Sysbios application.
According to spruh18e.pdf (page 400) " Auto-conversion must be enabled when using TBPRDHR" , so I did.
My program is intended to call SFO() to calibrate MEP_ScaleFactor.
When compiling I encounter
W: #10247-D creating output section "Cla1Prog" without a SECTIONS specification W: #10247-D creating output section "CpuToCla1MsgRAM" without a SECTIONS specification E: #10099-D program will not fit into available memory. placement with alignment/blocking fails for section "codestart"
It seems as if SFO_TI_Build_V6b_FPU.lib makes use of CLA, but CLA is not configured in linker command file TMS320F28069.cmd.
Is there an example showing how to use HRPWM with auto conversion in SYSBIOS?
Is it feasible to use auto conversion without using SFO()?