Hallo everyone,
I am working with the TMS320F28377D and just tried some of the example projects I found in the controlSUITE. In the file F2837xD_SysCtrl.c there is the function InitSysCtrl() with the line:
InitSysPll(XTAL_OSC,IMULT_20,FMULT_1,PLLCLK_BY_2); //PLLSYSCLK = 10Mhz(OSCCLK) * 40 (IMULT) * 1 (FMULT) / 2 (PLLCLK_BY_2)
The value of IMULT in the function call does not fit to the value in the comment. Does this mean, the microcontroller is running with 100MHz instead of 200MHz?
I called InitSysPll with IMULT_40 and tried to run the project blinky_dc_cpu01. But that did not work.
I hope you can help me.
Yours,
Robert