Hi,
I´m using the McBSP A (GPIO20-23) in SPI Mode to connect a Serial MRAM.
Commissioning of my HW showed that the clock duty cycle (MCLKXA, GPIO22) is not 50/50, but the high/low phases are a multiple of LSPCLK cycle time (75MHz --> 13.33ns).
In our configuration with 25MHz SPI Clock, the duty cycle is 1xHigh/2xLow.
I could not find anything about this behaviour in the data Sheets (SPRS581D and SPRUFB7B).
Technical this is not a Problem, but I want to know if the low Phase of the clock is always the longer one when the baud rate has an odd divider to LSPCLK.
Regards, Peter Fritzenschaft