Hi,
I am trying to use the Motorware examples (labs) using a F28027F launchpad but all of them cause the processor to get stuck when executin HAL_Init.
I have tried with and without the Boost-XL and external power supply and the result is always the same.
I have tried CCS v5.5 and c6.01, both with the latest Motorware.
Stepping the program in assembly, the problem seems to start at a LCR command is executed with an operand pointing to a memory mapped area or a location with FFFF (ITRAP) in it.
Please note that I have removed the optoisolators on the launchpad and connected directly the JTAG, power and UART signals. I cannot remember if I had tested the labs before that, but I do not see how this could affect the result, especially when providing all power from USB.