I try to copy the code about firmware flash request message in "PRIME Host Message Protocol Specification".
MSG_TYP = 0x14; //GET_INFO
MSG_ORG = '1'; //originated from PLC
MSG_RPY = '0'; //need reply message
MSG_BDY = uint16_t blob_id; // blob id to identify the blob
uint16_t blob_len; // length in bytes of blob to read
uint16_t blob_addr; //start address of the blob, only exist when blob_id=4
And to get information in F28069.
But I don't know what is the next step after coding?
Is using the C2prog to flash the code into F28069?
Best regards,
Wayne