On the C28335, there was example code on relocating the 28335 Flash library to RAM, as follows:
Flash28_API:
{
-lFlash28335_API_V210.lib(.econst)
-lFlash28335_API_V210.lib(.text)
} LOAD = BOOT_CODE,
RUN = RAML0,
LOAD_START(_Flash28_API_LoadStart),
LOAD_END(_Flash28_API_LoadEnd),
RUN_START(_Flash28_API_RunStart),
PAGE = 0
Now I need to do a similar task with the 28377D; I downloaded the latest F021 Flash API, and I have integrated it, but I need to relocate the Flash library either to a specific Flash segment or ideally to RAM. I have looked through all of the reference documents and source code, but I could not find a similar example on how to relocate this new library. There also do no appear to be any "LoadStart" references in the F021 header files to use.
Thanks,
Jim