I have a TMS320F2808 board design with a working code set that I inherited from several engineers no longer with my company. I need to make a few changes to the code which I've done and compiled the code and got it loaded into flash using an existing exdsp200 script. The code does a CRC check at startup. From comments in the source code I need to update the CDC value manually based on the value read from the emulator.
The design was done with CCS v3.3 and never migrated. I am trying to migrate to CCS v5.5.
I have a Spectrum Digital C200 XDS510LC emulator. I've used the SDConfig utility provided with the emulator to reset and test the emulator and to verify the connection. All successful. When I use CCS to run the debugger, I get "C28xx: Flash Programmer: Device is locked or not connected. Operation cancelled."
As a sanity check I imported the existing code (at least the source code, the project was not archived) with no changes and I get the same result.
There's something I don't understand here and I'm hoping I've got a setting wrong or something. I know the hardware and firmware work. I just need to get the build process ironed out.
Can someone please help?