I just noted that the flash wait state settings used by the F2802x v2.10 drivers appear to be different to ones I had been using previously that I think original came from a project based of the blinking LED example project.
My older projects use:
Paged read wait states (FBANKWAIT.PAGEWAIT) = 3
Random read wait states (FBANKWAIT.RANDWATI) = 3
OTP wait states (FOTPWAIT.OTPWAIT) = 5
Whereas the newer settings are 2, 2 and 2 respectively ...
I tried perusing the device datasheet but table 6-51 seems to mandate using 2, 2 and 3 respectively
Which set is correct??
Thanks