In the process of developing boot loader and on board programming code a recent attempt at reprogramming flash resulted in a locked Flash indicated by the message:
C28xx: Flash Programmer: Device is locked or not connected. Operation cancelled.
I have read in other posts that the boot pins can be configured to change the boot mode and then re-gain access to the flash device. Our device is soldered onto a controller board and we have no direct to access to the TRST and GPIO boot select lines without removing the device from the board.
Is there no other method to unlock the flash?
Thanks in advance,
Doug R.