I'm working with Code Composerr Studio, and I'm struggling with programming the external SPI Flash, from which I wanna load the program at start-up via SPI-A boot mode.
A hint would be great!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm working with Code Composerr Studio, and I'm struggling with programming the external SPI Flash, from which I wanna load the program at start-up via SPI-A boot mode.
A hint would be great!
Hi Christian,
christian affolter said:A hint would be great!
Here's an app note, but I'm not sure whether the same can be adopted for F28335, do check:
3482.SDFlash2834x_EEPROM_Flash_Programmer_Readme_V1_0.pdf
Regards,
Gautam
Hi Gautam
thanks a lot for the answer - this will be the way to do it.
on http://emulators.spectrumdigital.com/utilities/sdflash/ the supported processors are listed and the F28335 is one of it.
I'm asking me now if I really have to wite the Driver by myself or if there is one at disposal by TI.
And a general question : what is the state of the art to uBoot a uC ike F28335
Hi christian,
This app-note may also be helpful:
http://www.ti.com/lit/an/spraaw0/spraaw0.pdf
I think that I'm now on a good way....
the SPRAAL3 (Flash Programming Solutions for the TMS320F28xxx DSCs) helped me.
There I found the key words "Flash API" --> source in "setup_Flash2833x_API_V210.exe"