Hello all,
If the following configurations are made:
SOC0 - ADCINA0
SOC2 - ADCINB1
And SOC0 and SOC1 happen at the same time, which of the following events (if any) will happen?
1) ADCINA0 is sampled to S/H-A and ADCINB1 is sampled to S/H-B at the same time. Then, ADCINA0 is converted (because SOC0 has priority), then ADCINB1 is converted.
2) ADCINA0 is sampled to S/H-A and then converted. Then ADCINB1 is sampled to S/H-B and then converted.
My problem is that in my system, SOC0 and SOC2 may or may not happen at the same time. If they do happen at the same time, I need them both to sample as quickly as possible. Unfortunately, I can not use the simultaneous sampling feature since the two will not always happen at the same time.
Thanks in advance!
Edit: I am using the Piccolo 28035.