I am working on the design of a board using the 28034 where I have 7 inputs that are interrupts. Reading through the "Piccolo System Control and Interrupts Reference Guide" (SPRUGL8C), I noticed that Figure 79 (page 120) shows the GPIO0~31 pins connecting to XINT1, XINT2 and XINT3 through 32-to-1 multiplexers.
Am I correct in thinking that the three interrupt signals ,XINT1~3, are "normally" connected to GPIO12, 16 and 17? SPRUGL8C seems to indicate that only 3 of the 96 interrupts can come from the GPIO pins.
Thanks in advance.
Phil