I am using ADCINA7 (pin J5.3) to measure the voltage from a pressure sensor (after being amplified by an INA333).
Attachment shows : Voltage (mV) after an exponential curve has been subtracted
I am noticing unexpected spikes that are most noticeable in attached picture.
I wish that I had the option of increasing the gain of the INA333, but that is not possible with my application.
A former TI employee that I spoke with suggested that I use a 10 bit ADC instead of 12 bit ADC to prevent these spikes from occurring. At the time, this seemed like a great idea but, upon looking into it, I became uncertain if this is a possibility. Also, I am uncertain how to actually change the code so that it only uses a 10 bit ADC.
I would appreciate suggestions either to convert the 12 bit ADC to 10 bits or other ideas of how I might remove these spikes.
Thanks for the info!