We are working to develop a solution using the F28M36x concerto device. The control card development kit hardware is working well but we cannot open the schematic capture file (F28M36x_180controlCARD_R1.1.sch) provided by TI because it is a binary file in PADS. We cannot import these files into our design software which is currently Altium 2009 (they appear as blank screens).
The import would work if the files were saved in the more generic PADS ASCII format. Could the schematics be released in ASCII so we can speed our work? We would like to thank TI for providing the schematics and hope to be able to use them as a head start on our own board development.
Many Thanks,
bradford@audio-3.com
C2000 32-bit Microcontrollers Forum: Request to release F28M36x_180controlCARD_R1.1.sch (found in ControlSuite)