Hi folks,
I will be migrating a control equipment for induction motors from closed loop slip control to instra spin Texas- instruments platform.
Here are my questions:
The current implementation has a tachogenerator with a resolution of 9 Pulses per shaft rev. Would this provide decent results or would I be better off using sensorless feedback?
We currently have all the power stage equipment and current driving sensors required, and will only be replacing the control unit. I would like to know if there is any difference in using one of the control cards, such as the Piccolo TMS320F28069M or if a launchpad board, such as the F28027D development board could be used. Also, where can i find specs relating to where the signals go, for example current sensors, voltage divider for the DC-Link, etc?
Is there any model of CPU that I should aim for or will the 28027 be enough? The equipment is torque driven, rather than speed and should be able to offer dynamic braking.
Grateful for any clarifications
picolo boards