Delfino Evaluation Board TMDXDOCK28377D Example Project Errors
Hello,
I tried to build the Example Project "sdfm_filter_sync_cla_cpu01/cpu02" and it failed.
Errors are:
- #10010 error encountered during linking
- #10234-D unsolved symbols remain
- unresolved symbol _GPIO_SetupPinMux, first referenced in ./sdfm_filter_sync_cla_cpu02.obj
- unresolved symbol _GPIO_SetupPinOptions, first referenced in ./sdfm_filter_sync_cla_cpu02.obj
And Warnings are:
- #10063-D entry-point symbol other than "_c_int00" specified (should be no problem as FAQ says)
- #1107-D conversion from integer to smaller pointer in line 58…61 and 89…92
I tried to build on two computers with two independent installations:
Windows7
CCS Version: 6.0.1.00040
Compiler Version 6.2.7
Windows8.1
CCS Version: 6.0.1.00040
Compiler Version 6.2.7 and 6.2.9
Is there a solution for me? Had these Problemes earlier on other Projects while combining SDFM Project with USB fuctionality. It still wont work unfortunately. If needed i will add a logfile, but i think it is not usefull in this case.