Hi All,
I can;t generate a TZ5 action/ I'm having a very simple testcase for triggering a trip but without result:
All mux-inputs of EPWMXBAR5 are disabled.
The TZEL.bit.CBC5 is enabled for EPWM1.
I now start (manually) toggle the EPwmXbarRegs.TRIPOUTINV.bit.OUT1, but I don't see the EPwm1Regs.TZCBCFLG.bit.CBC5 being set.
PWMs are enabled and clocksources are enabled. I can trigger CBC1 by using InputXbar1 (TrigRegs.INPUT1SELECT).
Could someone verify that this is not a HW bug and that I'm doing something wrong? Or can I only route this through the DigitalCompare module?
Best regards,
Tjarco