Hi everyone,
Where can I get G3_HostAppliction.exe this software?
Inside the "TI G3 Power Line Communication Developer's Kit Design Guide" has mention this software.
But I can not find where I can download it.
Is anyone know it?
Wayne
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Wayne,
wayne lu1 said:Where can I get G3_HostAppliction.exe this software?
You should get it over here: http://www.ti.com/tool/ti-plc-plclite
Regards,
Gautam
wayne lu1 said:But is Zero-config GUI the same as G3_HostAppliction?
I'd the same doubt too but it seems so... check this link: http://processors.wiki.ti.com/index.php/Smart_Grid_PLC_FAQ#Zero-Configuration_GUI.2FHost_Application
Seems like G3-HostApplication has been renamed as Zero-config GUI.
Regards,
Gautam
Wayne,
I have four versions from several PLC development packages. You can download this archive 4113.PLC.rar.
Regards,
Igor
Igor Gorbachev said:I have four versions from several PLC development packages.
Thanks for the link, Igor!
Igor,
Thanks for your help.
But how do I use these packages?
Do I need to import these packages to the PLC kit through the CCS?
Cause I only know there are many code but I don't know how to use them.
Regards,
Wayne
Wayne,
when you unpack RAR you can see four folders with HostApplicationEmulator projects for Visual C++. There are G3_HostApplication.exe or HostApplication.exe files into "Release" folders. You can try any, but for your case may be better take executable files with prefix G3.
Regards,
Igor
Igor,
I reading chapter 4 of this file. http://www.ti.com/lit/pdf/tidu237
But I don't know how to do with what you gave to me.
Thanks,
Wayne
Hi Igor
I have run G3_HostApplication.exe and Host_CLI.exe which you gave to me.
But both of them have some problem.
This one is after running G3_HostApplication.exe.
And this one is after running Host_CLI.exe.
Both of them I can not give the command.
And it seems there are some errors but I don't know how to do with these errors.
Wayne
Wayne,
I think you need to refer to user's manuals of these applications and you should apply needed arguments of command line when you run these applications. At least "port" can't be 0 at your first screen shot. It should be matched with connection port of your PC and KIT.
Regards,
Igor
Hi, Wayne.
wayne lu1 said:And someone told me I need to load the G3 codes into the controller in advance.
But I don't know what is the G3 codes too.
Let us in order.
UG (p.37) : "The latest G3 binary should be flashed onto the F28069"
UG (p.3): "The development kit includes the following software:
• G3 PLC Binaries
– G3 PHY and Lower MAC Project Binary Image
• (g3_plc_FF2806x_AFE031.out for F28069)
• (g3_plc_F28M35x.out for F28M35x) "
Thus you need to use the pre installed original firmware of your KIT. If you have uploaded some custom binary then you should return to original binary. I suspect there is connection problem. Open device manager on your PC and check # of COM-port connected to KIT. This # is argument "Serial Port assignment" when running HostApplication (Table 7, p.4.2 of UG). You can use SCI-B (USB-connection) as well as SCI-A(nul-modem connection) of your KIT.
Regards,
Igor
Hi Igor,
I tried two kinds of binary code which are
C:\Texas Instruments\G3_SDK_Package_V7_4_1_6\SW\Bin\sysbios_g3_plc_aes_F2806x_AFE031_CRC16_MSB_LOADNG_image.hex &
C:\Texas Instruments\PRIME_SDK_PackageV8010\SW\bin\v8.0.1.1\prime_iec432_f2806x_image.hex.
They can work in GUI, but I can not understand why they can not connect on G3_HostApplication.
It still shows unable to open com port.
Regards,
Wayne
Wayne,
you are right, I have the same problem with running g3_HostApplication from 7150 development package. Try hostappemu.exe from 7710 package (refer to folder 7710 of my RAR which has been uploaded before). I have checked this application and one works for me at least.
Regards,
Igor
Wayne,
wayne lu1 said:
I had try 7710 package.
But the hostappemu.exe just flash a second and close.
it's strange,
did you run hostappemu.exe with CMD.EXE (Start->CMD, and then command line "......\hostappemu.exe" with needed arguments)?
Regards,
Igor
Hi, Wayne.
wayne lu1 said:Hi Igor,
I run what you told me, and it shows
HostAppEmu: Version: 3.10.0.6 - Product Version: 3.10.0.6
ERROR: multiple modes specified.
What is this mean?
It means you didn't apply argument for selecting mode (P2P or MAC). Pay attention at following screen shot where argument "/?" was applied:
and, for example, now we can select comport 1 (argument "-port 1") and point-to-point mode (P2P - argument "-x"):
no one modem is connected to my PC here and my PC haven't COM1. An application was finished on timeout.
Happy New Year and good luck!
Regards,
Igor
Hi Igor,
Happy New Year.
I had do what you told me.
I gave the command( -p 10 -x), and it showed like this fig.
But it just stop at here.
I could not give any command after this.
And I didn't see where I can read the product id(PID) or change the PID.
It is different from what the guideline says.
Regards,
Wayne
Wayne,
First, at your screen I see the following:
Device Type G3
PHY Mode PRIME
There is something wrong. I suspect your original firmware is "G3". Try other set of arguments:
-p 10 -g n
Honestly I didn't try this application "in detail". Again run it with argument ''/?" and learn all available arguments. Try different sets of arguments. When you will try arguments, pay attention on a version of supported protocol which is provided by original firmware of your KIT. In fact the original firmware provides only one (G3 or PRIME). Verify this thing.
Regards,
Igor