Customer is running the “usb_dev_msc” example application on the TMS320F28377 Experimenter Kit. They have been running the example with the USB OTG cable and flash drive connected to the micro USB port on the control card and a regular USB cable connected to the USB mini port for a virtual COM port. I am able to run all of the commands (“cat”, “ls”, etc.) provided in the example code successfully.
They need to be able to write data to the flash drive. The first attempt at writing using calls to f_open() and then f_write() have been unsuccessful (the code hangs waiting for the write to complete). Can you send me the sequence of file system calls that I need to make in order to write to the drive including any calls to configuration functions that are specific to setting things up for write operations?
Thanks,
Mark