I have just received a c2000 Piccolo as a gift, but I only have a MacBook Pro. Is there any way I can
program my controller using a MAC OS?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have just received a c2000 Piccolo as a gift, but I only have a MacBook Pro. Is there any way I can
program my controller using a MAC OS?
Actually...You can program the C2000 LaunchPad using Mac OSX. Energia version 14 was just released a few days ago and includes support for this LaunchPad in OSX. You can get it here.
We are working on releasing a version of CCS for Mac. It should be released sometime next year.
BR,
On the other hand the MSP430FR5969 was recognized with no issue at all... and after a simple update, I was able to successfully upload sample code.
I an using a MacBook Pro running Yosemite. I have installed Energia Version 14 for Mac OS X.
Sorry I didn't see that. If there are no serial ports available, try downloading and installing these drivers:
http://energia.nu/files/EnergiaFTDIDrivers2.2.18.zip
The drivers for the XDS100 were supposed to be rolled into this package, but I haven't had a chance to check.