Im using simulink to program code to flash memory, However every time I build the project it shows the following error:
The build process will terminate as a result.
Error while loading and running the program.
The TI flash API library does not exist on your machine. Specify the right path or download the appropriate flash APIs from TI's website or TI's controlSUITE installer.
I have installed the flash api tool on my pc to use flash memory, however i cannot specify the API folder location in the configuration parameter in simulink (every time i do it and click apply and ok, it just resets to its default location).
Also I dont know how to program flash memory using code composer studio 6. Do i have to set a specific jumper from the board or something like that? Im using the c2000 launchpad F28027. Please help!