When attempting to flash a TMS320F28377D I get the following errors:
C28xx_CPU1: GEL Output:
Memory Map Initialization Complete
C28xx_CPU1: Loader: One or more sections of your program falls into a memory region that is not writable. These regions will not actually be written to the target. Check your linker configuration and/or memory map.
C28xx_CPU1: File Loader: Data verification failed at address 0x00082000 Please verify target memory and memory map.
C28xx_CPU1: GEL: File: C:\Development\UK11sa010\Tesla\Main\DSP\V5DSP_CORE_1\Debug\V5DSP_CORE_1.out: a data verification error occurred, file load failed.
I also tried changing the project to run from RAM and got similar errors. This appears to be a problem with verification. When I try programming into RAM with verification turned off I get the following:
C28xx_CPU1: GEL Output:
Memory Map Initialization Complete
C28xx_CPU1: Trouble Setting Breakpoint with the Action "Finish Auto Run" at 0x8f91: Error 0x00000008/-1066 Error during: Break Point, Cannot set/verify breakpoint at 0x00008F91
C28xx_CPU1: Breakpoint Manager: Retrying with a AET breakpoint
Any ideas what may be wrong?
Thanks and regards,
Adam