I read on page 1815
SPRUHM8C–December 2013–Revised December 2014
and I don't understand Table 15-9. ECCTL1 Register Field Descriptions.
field PRESCALE has 5 bits, so max value is 2^5-1 = 31, but I read 64h,65h 2b66 ??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I read on page 1815
SPRUHM8C–December 2013–Revised December 2014
and I don't understand Table 15-9. ECCTL1 Register Field Descriptions.
field PRESCALE has 5 bits, so max value is 2^5-1 = 31, but I read 64h,65h 2b66 ??
Hi Mauro,
The Description for PRESCALE should say:
---
0h (R/W) = Divide by 1 (i.e., no prescale, by-pass the prescaler)
1h (R/W) = Divide by 2
2h (R/W) = Divide by 4
3h (R/W) = Divide by 6
4h (R/W) = Divide by 8
5h (R/W) = Divide by 10
...
1Eh (R/W) = Divide by 60
1Fh (R/W) = Divide by 62
---
I will file a bug so that this issue can get resolved.
Thank you,
Brett