Hi all,
I have some basic doubts on CBC ( cycle by cycle) control on Trip zone module.
If the fault pin comes low from the gate driver ( or some external circuitry and the fault pin is connected to Trip zone XBAR pin), the pwm pulses will behave accordingly to their choice given in TZCTL register. I am configuring cycle by cycle trip limit.
I have the following queries : -
1. will the PWM will behave normally ( i.e. according to the logic) at next rising edge of pulse.?
2. For how many cycles these phenomena can be configured. Is there any option for doing so?
Regards
Raja Saha