This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Connecting 14-Pin JTAG emulation header to Concerto MCU

I'm designing a motherboard for the F28M35x Concerto MCU which will include a 14 pin JTAG header for programming.  I'm designing to schematic 2-17 from the F28M35x Data Sheet but I wanted to verify the circuit because it's a little unclear from the drawing.  I've added some connection dots to the drawing where I believe they should go, but could someone please confirm they are correct. This is a critical circuit and I want to make sure there aren't any mistakes.


The drawing from the data sheet:

My drawing, including connection dots (please ignore the ref designators).  Are these connections correct?