Hi there,
I've got F28069 device and using few FIR filters included in TI Fixed point library.
Most of them are working but one in particular is not performing as expected (when compared with matlab results).
The filter is a FIR16 filter and calculated the coefficients using the ezfir16 file, which seems to be not included any more in the controlsuite (why is that btw?).
Anyway the filter I've designed is a fractional delay filter with 4 orders expecting to delay the input signal by close to 3 samples.
However the result constantly shows it's only delaying it by 2.
what could be the problem for this? other FIR filters such as a low pass filter are working as expected so it's really puzzling why this one doesn't work.
Please help!
Thanks,
Ayaka