Hi
In CCStudio, we can generate a hex file from the project and flash it to the controller.
In my application, I want to store the hex file in an external eeprom and then flash it to the controller flash.
Can I generate an encrypted hex file so as to protect it from reverse engineering when present in the Eeprom?
I came across an application called C2Prog to generate .ehx file which I understand is an extended hex file for encryption. I need to work on it further.
C2prog - http://www.codeskin.com/programmer
Is that the correct way or is there any other way ?
Attached is the user guide for c2prog
Thanks In Advance !
Smita