I use the TMDSHVMTRPFCKIT and program "HVACI_scalar" to run motor.
After the motor work a few seconds,the CCSv5.4 show that
"C28xx: Error: (Error -150 @ 0x0) One of the FTDI driver functions used during configuration returned a invalid status or an error. (Emulation package 5.1.73.0) "
When I try to close the error window ,the CCSv5.4 crash.
Any guidance and advice
Thanks!!!